This solution is one of the key techniques in predictive maintenance, often employed for les critical equipment where periodic check is sufficient. it allows obtaining information on equipment health at a predetermined Interval, for early detection of potential electrical and mechanical breakdowns.
Application areas
This service is suitable for propulsion and other rotating equipment above 22KW up to 500KW, pumps, compressors, turbines, fans. Also for the evaluation of electrical type faults, rotary frequencies, groove passage frequencies in winding, etc. It evaluates the source of more specific faults such as pump cavitation , parasitic frequencies
What we do
We agree with our customer and create routes with designated points to diagnose the main effects in order to arrive at highly reliable diagnosis such as mass imblances, misalignment, both rotating and structural clearances, bearing problems, as well as problems of electrical origin .
Thereafter a report is submitted with the following information:
- List of alarms values.
- List of global value measurements,
- List of deviations from the previous measurements,
- FFT graphs with views, exception reports of the values in alarms or deviations to be considered,
- Root cause recommendations or notes
Benefits
- Allows for early detection of machine faults such as component defects, alignment issues, and balance problems, so the problems can be addressed to avoid the complete failure of the machine
- Used to monitor the condition of the machine in order to determine in good time when to carry out maintenance on the machine to keep it in top shape
- Allows for preventive maintenance to ensure longer lifespan of the machines